cancel
Showing results for 
Search instead for 
Did you mean: 

ADC FAST CHANNEL AND SLOW CHANNEL

yang hong
Associate III

I am using NUCLEO-STM32H743ZI2, I notice adc channels has fast channel and slow channels. there are some sample rate limits on fast channel and slow channel? Can I mix to use them? for example , in2, in3, in4 and in7, in8, in9?

thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

Yes you can mix them. Just respect the minimum sampling time for each channel.

If you feel a post has answered your question, please click "Accept as Solution".