adc fails to initialize
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-26 8:18 AM
Board: stm32h753zi nucleo
Firmware & CubeMX: latest version
I have configured the adc to continous conversion and DMA output. The initialization fails in main.c in HAL_ADC_INIT. I stepped through the HAL lib and saw that LL_ADC_IsInternalRegulatorEnabled returns the HAL_ERROR.
The docstring of this function says
/* Verification that ADC voltage regulator is correctly enabled, whether */
/* or not ADC is coming from state reset (if any potential problem of */
/* clocking, voltage regulator would not be enabled). */
if (LL_ADC_IsInternalRegulatorEnabled(hadc->Instance) == 0UL)
I do not find any documents online which describe how the clock frequency of the adc should be set up. Could you please give me a hint.
Solved! Go to Solution.
- Labels:
-
STM32H7 series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-12 4:57 AM
I discovered my error. I have built some cpp classes as abstractions for io functionality. There is also an analog class in which I started the analog DMA transfer in the constructor. Then I created an global instances of this class so the constructor interfered with the ADC startup logic in main. I was sure that the error could not originate from my abstraction code because the fault already occurred in the CubeMX generated main.c, but I did not think of the constructor of the global variable also being called at startup.
Thank you very much for your help.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-26 8:43 AM - edited ‎2025-05-26 8:46 AM
You set the adc clock in clock tree ->
and then choose in adc settings...
+ in ds see the limits :
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-26 11:58 PM
Thank you for your answer.
In which document is this ADC table? I looked into the RM, PM and Nucleo 144 UM.
Also I tried different clock inputs (80, 64, 32, 16 MHz) but the error still occors.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-27 12:22 AM
>In which document is this ADC table?
in ds , as i wrote.
+
>but the error still occors.
To be true: i never seen this problem...but i dont have the H753 , i use H743 ; ( but its same chip , DIE450 );
So : if you get no warnings, when you "generate code" , then maybe a problem with the Cube/lib version;
i run IDE1.18.1 , + STM32CubeH7 Firmware Package V1.12.1 / 06-December-2024
Try update, if yours is old.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-28 1:18 AM
I also use STM32CubeH7 Firmware Package V1.12.1 and CubeMX v6.14.1
I do not get any warnings. I tried lowering the clock speed to 4MHz, but the error still occurs.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-05-28 2:57 AM
Did you any tests for ADC ok or not?
I would try:
Set in Cube ADC for a simple conversion: just one rank, on a channel, no dma, no oversampling, no continuous mode, just plain basic default settings.
Set ADC clock to any medium frequency for your vos range and core speed, maybe 20 MHz.
After init call ADC calibration,
Then call Hal ADC conversion in blocking mode...and tell , what comes out.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-10 7:00 AM
I was able to setup the adc in a separate project, but I am still unable to reproduce it in the original one.
The HAL ADC State reports as
272 = 0x110
which correspondents to
#define HAL_ADC_STATE_ERROR_INTERNAL (0x00000010UL) /*!< Internal error occurrence */
// and
#define HAL_ADC_STATE_REG_BUSY (0x00000100UL) /*!< A conversion on ADC group regular is ongoing or can occur (either by continuous mode,
external trigger, low power auto power-on (if feature available), multimode ADC master control (if feature available)) */
What could cause the internal error?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-10 7:18 AM
In addition all adc1 registers are set to 0.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-10 7:53 AM
Probably just wrong setting.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-10 7:54 AM
> all adc1 registers are set to 0
That usually means, that the ADC AHB clock is not enabled (ADC is a dual-clock peripheral, AHB clock allows to access the registers and kernel clock controls the converter itself). Check RCC_AHB1ENR.ADC12EN.
JW