cancel
Showing results for 
Search instead for 
Did you mean: 

ADC analog watch-dog interrupt

CAPOSIENA.Philippe
Associate II
Posted on March 18, 2016 at 15:43

Hello,

i want to use the analog watch-dog 1 interrupt with the STM32F334.

I configure the peripheral with CubeMx.

But the interrupt is never serviced. I must enable the EOC or EOS interrupt to get the Analog watch-dog call-back serviced.

I just use 1 ADC channel in continous mode (no trigger).

If i look at the registers when debugging, the flags for analog watch-dog are correct and the interrupt enable bit is set.

I don't know what to do anymore.

Is there a example ?

Thanks

Philippe
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on March 30, 2016 at 17:56

Hi Philippe,

1- Is the IRQ handler enabled in your stm32f3xx_it.c file?

2- Refer to the example STM32Cube_FW_F3_V1.4.0\Projects\STM32F302R8-Nucleo\Examples\ADC\ADC_AnalogWatchdog. It provides a short description of how to use the ADC peripheral to perform conversions with analog watchdog and out-of-window interruptions enabled.

You can take this example as start point to make required updates in the project generated with CubeMX for F334.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.