ADC after RST pin stm32
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-06 8:38 AM
Hi, I have a problem with the adc. I want to get
the voltage of the STM.
At the start up of my program I want to get the voltage of the STM. So I init the internal ADC and get VREFINT. I have the good value whit my calculation, so no problem there.
My problem is when I use the RST pin of the stm32. After rebooting the stm32 by using the RST PIN I read wrong value at the vrefint channel ( from 0 to 1500, or I used the oversampling mode so I must read value around 22700).
When I rebot the system electricaly, turn off and then turn on the power, the value is good. The problem is only when I used the RST pin.
Do you know where is the problem ?
Thanks !
Sorry for my english ...
#adc #reset #stm32l- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-06 9:59 PM
Hi, David,
VREFINT(regulated internally) is quit different from VDD or VDDA, right? So it may not be a good idea for using VREFINT to know VDD or VDDA.
As for the strange result after reset.....
I just use CubeMX and nucleo stm32F303 to make a quick check.
...
SystemClock_Config();
MX_GPIO_Init();
MX_USART2_UART_Init(); MX_ADC1_Init(); printf(''System Restart!\r\n'');while (1)
{ HAL_ADC_Start(&hadc1);HAL_ADC_PollForConversion(&hadc1, 20);
adcResult = HAL_ADC_GetValue(&hadc1);
printf(''VREFINT Value is %d\r\n'', adcResult);
HAL_Delay(500);
}It seems okay without the strange result you've described. (I use the onbard reset button.)
So there could be some problem in your reset mechanism...circuitry or something.
Good luck!
:(
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-07 12:19 AM
Thanks for your responses.
I use a stm32l0, and to reset the mcu I have a mechanism with a button where I need to push it 15 sec. The reset works.
I also noticed that when I flash my board with ST link, I have the same problem (the RST pin flag is set when I flash the board, so I supposed theRST pin is used by st link).
Next, I tried to make the conversion without the oversampling, and most of the time I get 2 in in the register of the ADC ... but when I electrically restart the STM, I have the same value as
Liu.Zhitai
.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-07 1:23 AM
... ( from 0 to 1500, or I used the oversampling mode so I must read value around 22700).
This makes me guess the OP was speaking about the 16-bit Sigma-Delta ADCs, of which the F303 has none.
It would be great if he (the OP) would be a bit more precise about his hardware and environment ...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-07 2:59 AM
with a button where I need to push it 15 sec.
To reset the mcu after a button has been pushed 15 sec. I would use external interrupt and timer to fulfill this detection and then called NVIC_SystemReset();
You may use oscilloscope to check your button circuitry and reset pin while you are pushing the button, perhaps you will discover something. Good Luck!