2015-10-05 4:24 AM
hi all,
ive written this sample code for receving data and storing in bufferhow do i stop receiving data when enter button is encountered#include <stdio.h>#include ''main.h'' static const char String1[] = ''ENTER THE OPERATION\r\n'';static const char String2[] = ''YOUR OPERATION IS:'';static const char String3[] = ''NUMBER 1 IS:'';static const char String4[] = ''NUMBER 2 IS:'';static const char ErrorString[]= '' YOUR CHOICE IS INCORRECT\r\n''; void USART1Configuration(void);void OutString(const char *s);char GetChar(void); void CALCULATOR(void);void START(void);void RECEIVE(void);void TEMP(void);int IN[100];int i=0;int main(void){ if (SysTick_Config(SystemCoreClock / 1000)) { while(1); } STM_EVAL_PBInit(BUTTON_USER, BUTTON_MODE_EXTI); STM_EVAL_LEDInit(LED3); STM_EVAL_LEDInit(LED4); STM_EVAL_LEDInit(LED5); STM_EVAL_LEDInit(LED6); USART1Configuration(); while(1) { CALCULATOR(); }} void USART1Configuration(void){ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE); GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1,ENABLE);} void OutString(const char *s){ while(*s) // Not NUL { if (USART_GetFlagStatus(USART1, USART_FLAG_TXE) != RESET) // if it's empty USART_SendData(USART1, *s++); // Out char, and advance }}void OutInt(const int *s){ while(*s) // Not NUL { if (USART_GetFlagStatus(USART1, USART_FLAG_TXE) != RESET) // if it's empty USART_SendData(USART1, *s++); // Out char, and advance }}char GetChar(void){ char ch; while(USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET); // wait while no data ch = (char)USART_ReceiveData(USART1); return(ch);} void CALCULATOR(void){ START(); RECEIVE(); TEMP();}void START (void){ OutString(String1);}void RECEIVE (void){ while(1) { IN[i++] = GetChar(); if ((IN[i]== '0x0d') || (IN[i]== '0x0d')) return;}}void TEMP (void){ OutString(String2); OutInt(IN);}#ifdef USE_FULL_ASSERT/** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ /* Infinite loop */ while (1) { }}#endif2015-10-05 5:40 AM
You probably want to test for 0x0A and 0x0D, not 0x0A twice.
You must properly NUL (0x00) terminate strings passed to other string functions.2015-10-06 12:01 AM
the 0x0d twice was a typing mistake sir,
however the main issue was writing the hex values 0x0d and 0x0a inside the braces. '0x0d 'and not simply 0x0d.figured that out yesterday.thanx for the help though sir.just one more query.do you have the code for rtc initialisation for stm32.wat i have in the snippets packet is based on register level programming.wat i want is the initialisation based on library functionsthanks in advance