2017-11-13 1:26 PM
Where to find the ACIM FOC library for STM32 ? When it will be in the STM32Cubexx ?
2017-11-14 5:40 AM
Hi
Cinelli.Antonio
,Your request is transferred to our CubeMX who can decide if such request may be considered in new tool features.
Thanks for sharing.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-02-15 1:36 AM
Hello,
Are you aware of this library :
http://www.st.com/en/embedded-software/stsw-stm32100.html
?The STM32 PMSM FOC SDK(STSW-STM32100), which includes the PMSM FOC FW library and ST MC Workbench, allows the user to evaluate the STM32 performance in applications driving single or dual Field Oriented Control of 3-phase Permanent Magnet motors (PMSM, BLDC).
You can find the full description on Motor Control Software Development Kit in
.I am pretty sure it will help you.
BR. Jeanne