cancel
Showing results for 
Search instead for 
Did you mean: 

About the SAI duplex mode of STM32F746

13603052469
Associate
Posted on October 29, 2015 at 10:56

Hi,my friend, 

I want to implement the both TX/RX channel of SAI, but can not find any code sample in STM32CUBE. I want to use DMA to transfer audio data between SAI and codec and start the TX/RX DMA at once and just use one DMA interrupt callback to process data. Now I can run the SAI_AudioPlay sample to play audio file on my board and which just use the SAI1B, working in slave mode. I add some code to init the SAI1A as the SAI1B, but found no data recieved in the RX buffer, but TX is work fine. Any one could help me ? Many thanks!

#sai-stm32f7
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0