2018-11-21 2:27 AM
Hi,
We tested to rewrite the data into STM32L433CC.
May i know why this device is unable to program data in second time?
If i use STM32F072, and it is able to rewrite the data in second time.
What is the different?
For example, i write the data at address 0x0000 to 0xFFFF, and the data is 0xFF at address 0xC000 to 0xEFFF. if i want to write data at address 0xE000 , i found the data is unable to be written at address 0xE000. But STM32F072 is able to be written on the same condition.
Thank you.
2018-11-21 2:53 AM
STM32L4 writes flash memory in blocks of 64 bits with 8 bits of ECC error correction code. So you can not write a second time to flash. L0 has no error correction, so you can write a second time.
2018-11-21 2:53 AM
STM32L4 writes flash memory in blocks of 64 bits with 8 bits of ECC error correction code. So you can not write a second time to flash. L0 has no error correction, so you can write a second time.
2018-11-21 2:56 AM
Thank you for your information and great support.