cancel
Showing results for 
Search instead for 
Did you mean: 

About stm32f107 and IEEE1588

zchongnari2
Associate II
Posted on May 29, 2011 at 08:21

Hi,

I find there is no applictation note about how to use IEEE1588 on stm32f107. As a newbie, it is very hard to start.

When i enabled the timestamp function, and adjusted the ethernet receive processing, but the ethernet was dead.

Who can tell me how to initialize the timestamp and the ethernet correctly?
1 REPLY 1
Thomas_Socomec
Associate II
Posted on March 12, 2013 at 08:44

Hello,

I have exactly the same problem with a STM32F207.

When I enable the CPU timestamp, I have a strange behavior with Ethernet controller : the MAC register tells me that the DMA never start (

ETH_DMABMR->SR is never set to 0).

Thank you in advance for your help.

Best regards,

Thomas