User Activity

Posted on April 18, 2013 at 14:13Hello everybody, I have a board with stm32f207 and I use GPIO_AF_OTG2_FS as USB device connection, and I have sometime a strange problem when I plug the USB cable. When I plug the cable, all is working correctly and ...
Posted on March 19, 2013 at 13:39Hello, I have a problem with ST flash loader demonstrator when I try to flash for the first time a STM32F207IG. I use UART1 and BOOT0 pins. ST flash loader detects correctly the microcontroller, and starts the erase ...
Posted on March 15, 2013 at 09:28Hello everybody, I have a question about USB device in VCP mode. I would like to keep my VCP communication open after a microcontroller reset (STM32F207). Is it possible ? In example, I have a terminal software runni...
Posted on March 12, 2013 at 10:07Hello, I have a problem when I try to connect IAR to the STM32F207 by the JTAG protocol. I have no problem when I use SWD instead of JTAG. I made a test with a J-Link probe and the SEGGER J-Flash ARM software, and I ...
Posted on July 11, 2012 at 09:14Hello everybody, I'm using the STM3210E Eval board with STM32103ZGT6 �C. I'm currently doing any tests in order to determine the quickest way of data transfer between external SRAM/NAND or external SRAM/SD Card. I wan...