cancel
Showing results for 
Search instead for 
Did you mean: 

6LoWPAN tutorial, GW not starting

Mathias Thorell
Associate
Posted on April 26, 2018 at 20:21

Hi !

I have tried to follow the steps listed in 

/external-link.jspa?url=https%3A%2F%2Fblog.st.com%2Ftutorial-6lowpan-guide-creating-network-sending-data-internet%2F

.

I got the same hardware mentioned there and I have managed to verify that I got the correct FW in my X-Nucleo IDW01M1; v160129. Finally, I have also moved the 0 ohm R4 -> R34.

However, I cannot get step 2 'Craete the Gateway' to work.

I have mounted the hardware and loaded the software and when I connect to it from my PC (using Putty) I see it hanging on

/********************************************************

* *

* FP-NET-6LPWIFI1 Function Pack v2.1.1 *

* X-NUCLEO-IDW01M1 Wi-Fi Configuration. *

* WiFi Bridge Application *

* *

*******************************************************/

(HAL 1.7.1_0)

Compiled Dec 15 2017 12:32:42 (KEIL)

Board UID: 006a004f3436510b36383230

Initializing the wifi module...

I have reset, re-uploade dthe software with the same result.

Since there is no makefile avialable for the GW softare (STM32CubeFunctionPack_6LPWIFI1_V2.1.1), I am unable to debug it to see where it's going wrong.

So my questions are:

  • Has anyone made the example gateway and node as describe din teh link above work ?
  • Where can I get the makefiel for the 

    STM32CubeFunctionPack_6LPWIFI1_V2.1.1 gateway software so I can build it myself in System Workbench ?

Cheers & TIA !

/T

null
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0