cancel
Showing results for 
Search instead for 
Did you mean: 

32F429IDISCOVERY

danieljackmorley
Associate II
Posted on March 22, 2016 at 18:20

Does this kit require a BDM to program the 

STM32F429ZIT6.  Or does it work through the USB?

I am new to ST products and what kind of tools do I need to use to program the device.

2 REPLIES 2
Nesrine M_O
Lead II
Posted on March 23, 2016 at 12:22

Hi morley.daniel,

Welcome to STM32 community 🙂

I'd highly recommend you to have a look to these two documents, they provide guidelines to novice users on how to build and run a sample application and to create and build their own application around the STM32F429 Discovery.

•

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00097320.pdf

•

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00092920.pdf

Also I recommend you to download the

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF259242?s_searchtype=partnumber

which is a graphical software configuration tool that allows generating C initialization code using graphical wizards.

-Syrine-

Posted on March 23, 2016 at 14:05

The DISCO board includes an SWD (single wire debug, like jtag, fewer pins) debugger, ST-LINK, provided by the F103 part on the board. This connects via the primary USB (mini), the target USB (micro).

The DISC1 model support mbed, and a virtual serial port.

The ST-LINK debugger is supported by Keil, IAR, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..