cancel
Showing results for 
Search instead for 
Did you mean: 

32F413HDISCOVERY - HS USB?

waclawek.jan
Super User
Posted on January 23, 2017 at 23:01

The 32F413HDISCOVERY  webpage, and also the data brief DocID029964 Rev 1, both say the kit has:

USB OTG HS with Micro-AB connector

however, the STM32F413 has 'only' an USB OTG FS.

Also, on the picture of the DISCO's PCB in the databrief it can be seen an overlay text 'USB_OTG_FS' next to said microAB connector.

Please comment.

Thanks,

JW

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee
Posted on January 24, 2017 at 09:58

Hi Jan,

Thanks for highlighting this discrepancy: you are right; only USB_OTG_FS is available in STM32F413ZH.

This is noted and will be fixed soon (in both web page and databrief).

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Amel NASRI
ST Employee
Posted on January 24, 2017 at 09:58

Hi Jan,

Thanks for highlighting this discrepancy: you are right; only USB_OTG_FS is available in STM32F413ZH.

This is noted and will be fixed soon (in both web page and databrief).

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.