cancel
Showing results for 
Search instead for 
Did you mean: 

16bit SDADC SIGMA DELTA STM32F373 doesn't work

sven
Associate II
Posted on September 06, 2016 at 20:06

Hallo,

I use the Mikroe compiler and don't get the SDADC for work :(

Is there a step by step manual, which values I have to use in which order?!

Maybe

1. enable SDADC

2. Initlialice

3. calibrate

or maybe

1.Init

2. enable?!

My Problem is, after

while (REOCF_bit == 0);

nothign happens....it seems that the SADC isn't running :(

1 REPLY 1
slimen
Senior
Posted on September 22, 2016 at 18:25

Hi,

You'll probably want to review as many SDADC examples as you can find under STM32CubeF3 firmware: 

STM32Cube_FW_F3_V1.6.0\Projects\STM32373C_EVAL\Examples\SDADC

You can get inspired from provided examples which can help you to develop and configure you application.

For more details about SDADC, refer to the chapter ''13. Sigma-delta-analog converter (SDADC)'' in the

http://www.st.com/content/ccc/resource/technical/document/reference_manual/fa/06/c7/15/3b/2a/4c/f1/DM00041563.pdf/files/DM00041563.pdf/jcr:content/translations/en.DM00041563.pdf

reference manual of STM32F37xxx.

Regards