cancel
Showing results for 
Search instead for 
Did you mean: 

1553 Bus handling with STM32F MCUs ?

aybala5
Associate II
Posted on December 17, 2014 at 20:11

Hi friends,

Is it possible to handle 1553 bus with stm32 series microcontrollers without using asic or fpga (ip core). For CANbus there are can trancievers that can be directly connected to mcu in the circuit, but for 1553 cant find any solution. Find an application but not understood how to connect to mcu.

application-notes.digchip.com/051/51-39510.pdf

Is there anyone tried to work with 1553 or knowledge to direct me. Thanks.

Thanks
2 REPLIES 2
Posted on December 17, 2014 at 20:44

The application is pretty niche, and specialized, so I doubt there's going to be a lot of resources to apply it to general purposes micros, especially those not rated for military or aerospace applications. Those using it, and with a lot of experience, likely work for the military-industrial complex, and aren't going to be discussing it with random people on the internets.

The HI-6110 would seem to have an FSMC type interface, but appears to need a lot of other dual memory resources. May be HOLT has a development board or FAE's you can talk with?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
aybala5
Associate II
Posted on December 17, 2014 at 21:27

Thanks Mr. Clive.