cancel
Showing results for 
Search instead for 
Did you mean: 

大家好,我最近在keil上使用STM32G0B1RE的芯片时,�?�现仿真时通过system viewer看�?到ADC的寄存器(�?示例图)(�?�有部分寄存器能看到,例如GPIO,IIC等),硬件用的是G0B1RE的NUCLEO�?�,请问有�?碰到过类似问题,还请帮忙解决一下,谢谢

fhu.11
Associate II

0693W00000DlYW2QAN.jpg

1 REPLY 1
Mohamed Aymen HZAMI
ST Employee

Hello @fhu.1​,

 I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.

"Hello, everyone, when I recently used the STM32G0B1RE chip on keil, I found that the ADC registers could not be seen through the system viewer during simulation (see the example picture) (only some registers can be seen, such as GPIO, IIC, etc.). The hardware is G0B1RE's NUCLEO board, has anyone encountered a similar problem, please help to solve it, thank you"

which Keil version are you using ?

Mohamed Aymen.