cancel
Showing results for 
Search instead for 
Did you mean: 

Micro SD whith micro controller

FuscoV
Associate

Good morning,

This is my first post

I' m searching for a special micro SD card with:

• MCU: 32-bit (produced by ST)

• MCU clock: > 100MHz

• RAM: > 384 Kbytes

• Flash: > 768 Kbytes

• Timer function

• Random number generator function

• Secure memory area required to store encryption keys

• Flash of at least 8Gb

• Sdk to develop and Upload software on microcontroller (ex: rsa and AES key generation function)

• Password or PIN for data protection stored on the flash (not for read but only for mofify/delete/create) 

Is there anyone who can recommend me some manufacturers please?

Thank you

Vincenzo

 

2 REPLIES 2
STTwo-32
ST Employee

Hello @FuscoV and welcome to the ST Community 

If you are locking for an STM32 with specific characteristics. I suggest you use the MCU/MPU selector included in CubeMX:

STTwo32_0-1706095915440.png

or the ST MCU Finder. Then, using the filters you can make the choice of product.

PS: What this mean "a special micro-SD card with: MCU: 32-bit (produced by ST)"

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

But does it have any option for, "an STM32 on a micro-SD Card" ?

 

EDIT: Ah - I see you've added::


@STTwo-32 wrote:

PS: What this mean "a special micro-SD card with: MCU: 32-bit (produced by ST)"


I think @FuscoV wants the STM32 embedded within the uSD card?