Hi,I can not help on the issue, but I can confirm same situation on SPIN3202. OCTH_STBY1 is reset and OCTH_STBY2 is set. No effect by comperator threshold setting in MCWB. You can try to set OCTH_STBY1 and OCTH_STBY2 again after MX init in /* USER CO...
Hello,let me add basic question related to this. Is there an example how to chainge from main position sensor (like hall sensors) to auxiliary sensor (like e.g. observer) during operation?Thanks
in other words:sensor displacement typical is 60° or 120° and it is same between H1 to H2 and H2 to H3. placement electrical angle is like offset of hall sensor arrangement to motor stator.