cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to create a FOC project with STM32G030C8T6 in STM32 Motor Control SDK

Gladson
Associate III

I am trying to create a project in STM32 Motor control workbench using STM32G030C8T6 microcontroller. I want to use a custom board for this project. I am trying to set all this by creating new power board and controller board and I also tried the inverter board option, but I am not able to generate a program with FOC algorithm for STM32G030C8T6.

I am able to create a custom inverter board, but when trying to use the inverter board in a project, then this is the error that I am getting.

Gladson_0-1741262052437.png

 

When I am creating a project using "Modular" hardware mode, and selecting power board and control board that I created, I am getting this error.

Gladson_1-1741262052438.png

 

Why am I getting this issue? and how can I solve this?

0 REPLIES 0