2014-06-20 8:40 PM
Hello all,
I,recently?want to migrate application base on library 2.0 of FOC from STM32F103 to STM32F051,and finally found the fowlling error:1:..\Output\svpwm.axf: Error: L6366E: mc_foc_methods.o attributes are not compatible with the provided cpu and fpu attributes .2:..\Output\svpwm.axf: Error: L6366E: mc_state_observer.o attributes are not compatible with the provided cpu and fpu attributes . Want to the help of the predecessors. #foc-2.02014-06-30 11:47 PM
Ciao yongfei.liu
My suggestion is to move to the new version of the MC library that supports STM32F051 Ciao Gigi2014-07-06 6:16 AM
2014-07-14 2:43 AM
Ciao yongfei.liu
I'm sorry, at the moment some parts of the code can't be released with open sources without a signed NDA with the customer and without a real businnes beyond. Ciao Gigi2021-06-28 2:58 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards