cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-SPIN3201, can't connect

Robert Wolfe
Associate
Posted on February 21, 2018 at 23:35

Hello,

I'm trying to connect to a steval-spin3201, but having no luck.  Both ST Motor Control Workbench and ST-LINK cannot find it.  If I look in the Device Manager of my PC, I see the 'STMicroelectronics STLink Virtual COM Port (COM4)', so the PC recognizes it, just that I can't connect.  

ST Motor Control Workbench says 'Connection failed! No response, check the communication cable, the power on the board or the baudrate', all of which I've done.

Please advise,

Robert

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards