cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-PTOOL4A : Error MC_DP_FAULT and Motor Profiler Connection Issue

JulesC
Visitor

Hello,

I am attempting to run a Brushless DC-Flat motor using the STEVAL-PTOOL4A board. However, the system fails right after entering the RUN state, returning an ERROR MC_DP_FAULT (via MC_GetOccurredFaultsMotor1).

To resolve this, I tried using the Motor Profiler to identify the exact motor characteristics, but I am unable to establish a connection with the board (see attached screenshot).Capture d'écran 2026-02-04 143222.png

Motor Characteristics:

  • Nominal Voltage: 12 VDC

  • Rated Speed: 10,000 rpm

  • Starting torque: 225 mNm

  • Rated Current: 2.18 A

  • Winding Resistance (phase-phase): 0.88 Ω

  • Winding Inductance (phase-phase): 0.331 mH

  • Pole Pairs: 7

Could you please help me identify the cause of the MC_DP_FAULT error and why the Profiler fails to connect?

Best regards,

Jules

0 REPLIES 0