2012-03-21 08:45 AM
Hello all,
I tried to use the USB to serial interface SDK for the STEVAL-PCC009v2 dev board to write a custom driver for the L6470 (EVAL6470 board). The included library SPI_SDK.dll works fine, but the command: DFU_GoTODFUMode() from the DFU_SDK.dll to get the board in DFU mode gives an undocumented error: 7 and does not work. Is there a solution for this problem?2012-07-09 02:58 AM
Hello all,
Unforalltunately i got no answer on my question.
I saw that there is a new patched version of the STEVAL-PCC009V2 firmware.
Does this address my problem?
It would be nice if there was at least a changelog with all these closed source firmware.
Greetings,Nils.
2021-06-21 09:37 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards