2016-05-13 6:18 PM
Hello
I try to use In-Wheel motor. 300W with Hall sensor.I used workbench and finally succeeded to run Motor Profiler .And got motor parameters, PID gains.After this, applied these parameters and tried to run the motor.But because of this error, it doesn't run. ''Start-up Failure''.I referenced some troubleshoot. and tried several things.Like decreasing G2 gain in observer. and increasing variance threshold in Observer+PLL. But still didn't work. I expected higher current like 1A when starting up. But my current metershows just 0.2A. Current meter just show overall current not just phase current though. Now what can I try? (Thanks Gigi for your big help)2016-05-16 4:02 AM
Ciao Lino
this seems a duplicate of the other post Ciao Gigi2021-06-27 8:53 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards