cancel
Showing results for 
Search instead for 
Did you mean: 

ST Motor Control Workbench V2.1

lumley
Associate II
Posted on April 03, 2013 at 02:56

Where can I find workbench version 2.1?

In a previous thread entitled ''

Has STM32 MC FOC SDK V3.3 released?'', the

ST Motor Control Workbench V2.1 is mentioned.

On this page, I found Version 2.0 of the Motor Control Workbench. Where may I find version 2.1?

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF257839

(Version 3.3 of Motor Control SDK is here:)

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257936

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
lumley
Associate II
Posted on April 16, 2013 at 00:30

Version 2.1 can now be found here.

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF257839?s_searchtype=partnumber

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards