cancel
Showing results for 
Search instead for 
Did you mean: 

ST Motor Control with STLinkV3

Thundernail2000
Visitor

Hi all,

I have adapted the B-G431B-ESC1 board into a custom design and I am using a STLINK-V3MINIE for programming. I can program the controller and I can communicate via the serial interface.

But ST Motor Pilot V1.2.12 does not detect the UART interface. The 'Board Connection' area is greyed out. I tried older versions of the MotorPilot but it did not work too. 

Can ST Motor Pilot not work with STLINKs or do I need a different one than the STLINK-V3MINIE?

 

Kind Regards
 Thundernail

1 REPLY 1
AScha.3
Chief III

Is in your system the serial port visible?

Did you connect to the serial port of mini E ?

 

If you feel a post has answered your question, please click "Accept as Solution".