cancel
Showing results for 
Search instead for 
Did you mean: 

source cord를 제공해 주실 수 있나요?

dentistkim
Associate

안녕하세요. 저는 개인 개발자 입니다. 이번에 steval ctm051 보드를 구입해서 srm 을 공부하려는 데 소스코드를 제공할 수 있다고 해서 어떻게하면 소스코드를 제공 받을 수 있는지 알려 주시면 감사하겠습니다.

Please note that the forum is English-speaking, which is why I have machine-translated your question into English:

Hello. I am an individual developer. I recently purchased the steval-ctm051 board and would like to study SRM. I was told that the source code can be provided, so I would appreciate it if you could let me know how I can obtain the source code.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @dentistkim, to the community!

You probably made a typo and meant the STEVAL-CTM015V1?
I had already answered the same question here, which has not changed since then.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @dentistkim, to the community!

You probably made a typo and meant the STEVAL-CTM015V1?
I had already answered the same question here, which has not changed since then.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.