cancel
Showing results for 
Search instead for 
Did you mean: 

PI控制调参

sunboy_351
Associate

sunboy_351_0-1703141662729.png

sunboy_351_1-1703141714429.pngMCSDK5.4.8版本 相最大电流270A,采样电阻0.0009欧,Lq 0.0991mH,Ld 0.04115mH,定子电阻0.01974毫欧,三电阻采样,相电流采样放大倍数3,电机相移角295度,PWM  16000Hz, 扭矩环调参后电机轴抱死,无法启动。

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
FBL
ST Employee

Hello @sunboy_351 

Correct me if this translation is incorrect.
> The MCSDK5.4.8 version has a maximum current of 270A, a sampling resistance of 0.0009 ohms, Lq of 0.0991mH, Ld of 0.04115mH, a stator resistance of 0.01974 milliohms, three-resistor sampling, a phase current amplification factor of 3, a motor phase shift angle of 295 degrees, and a PWM frequency of 16000Hz.

After adjusting the torque loop parameters, the motor shaft is locked and cannot be started.

 

Have you tried reducing the gains? Have you tried X-CUBE-MCSDK-6?

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


sunboy_351
Associate

BMS128-60H  Motor(Hall)

 

示例

参数值

 

示例

参数值

voltage platform

 

60V/72VDC

rated power

 

1.5kW

peak power

 

4KW

rated torque

 

4.1N.m

Peak torque

 

45N.m

peak current

 

270A(45Nm)

Max.speed

 

5400rpm

Ke

 

8.63V/krpm(线反电动势有效值)

POLE_PAIR_NUM

 

3

Lq

 

0.09991mH

ld

 

0.04115mH

Rs(line)

 

19.74mΩ

Max.fwcurrent

 

212ARMS

温度传感器型号

 

MF58-503F3950

Max.power

 

4kW

Max.torque

 

45Nm

 

 

 

 

 

 

 

 

 

rotational inertia

 

2.6g.m2

 

 

 

 

 

 

Motor parameter

Workbench:

sunboy_351_0-1703213299593.png

 

 

sunboy_351_2-1703213335038.png

 

sunboy_351_3-1703213357808.png

sunboy_351_4-1703213371086.png

sunboy_351_5-1703213386400.png

test

sunboy_351_6-1703213404268.png

1 first start  status  under voltage

 

sunboy_351_7-1703213497669.png

sunboy_351_8-1703213511163.png

2.clear  the  fault  next  start  

motor Vibration  status  Run  is not faults

sunboy_351_9-1703213657002.png

Stop-> next start:  motor is not rotate

sunboy_351_10-1703213688485.png

 

Open loop   motor Normal rotation

sunboy_351_11-1703214064385.png

I use STM32F103RBT6, 64MHz, the above problem occurs, how to find the problem point?