cancel
Showing results for 
Search instead for 
Did you mean: 

Perform high speed rotation on EVALKIT-ROBOT-1

ss.3
Associate

Hi,

I try to perform high speed rotation on EVALKIT-ROBOT-1, my target rotation speed is 6000rpm without loading.

I downloaded the example firmware "STSW-ROBOT-1", change values of "DEFAULT_TARGET_SPEED_RPM" and "MAX_APPLICATION_SPEED_RPM" from 4550 to 6000.

In main(), MC_ProgramPositionCommandMotor1() is directly called with parameters which equivalent to 6000rpm (run 2000*360degress in 20sec), 

then use MC_GetMecSpeedAverageMotor1() to track the motor speed, the maximum speed I got is around 3800rpm.

According to the document "https://www.st.com/resource/en/user_manual/um2653-getting-started-with-the-evalkitrobot1-stmicroelectronics.pdf", 

Table 10 states that the system with no load can reach 4550rpm.

Figure 7 shows that continuous operation speed can even be higher then 6000rpm.

I am using the original set of EVALKIT-ROBOT-1 hardware, It cannot even touch the official speed 4550rpm.

Should I change other configurations to achieve the target speed?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0