cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Profiler fails

dsystem
Associate II
Posted on May 21, 2018 at 16:58

My end aim is to use #Motor #profiler to workout my motor parameters. I have #nucleo-F302R8 and #X-nucleo-IHM08M1 boards.

I selected these two in Profiler, Connected My motor and Hall devices, Entered 4 Pole pairs and max speed as 4000RPM. Max current as 20A (Motor rated for 30A). Connected Power suppy of 12V/40A . Connected and started Profiling.

Motor moved approx a revolution and stopped. And the after a few minutes and fails. Shows Resistance, Inductance, Supply voltage and current.

What is I am missing ??

Regards

Vimal Amin

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards