Measuring speed of motor dc encoder in quadrature stm32f4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-09-09 8:42 PM
hello community,
i am doing a project related to the speed control of a dc motor, to measure the speed i am using an incremental encoder, to make my code i have used the tool STM32CUBEMX and activating the combined mode for reading an encoder, this stage works without problems, but to measure speed I have had several problems, I understand the concept of speed measurement at a theoretical level, but at a practical level I made a solution that works moderately well (works well at high speeds), for this I use an extra timer which I use to count the time and through interruptions I count the ticks of this timer, the problem is that I'm still a beginner and my codes are not quite good, usually after doing something and that works fairly well, I go straight to google to find a code that someone from the community and thus feedback my own codes, but the more I search among the community, I have less hope to find a code that implements this speed measurement with an incremental encoder using a stm32, besides, supposedly the implementation I made should work also for low speed, but it doesn't go well, that's why I ask if any of you have implemented something of this style and that it works. I would be very grateful if someone share some repository with this implementation, or someone could explain to me how to implement this being the most specific possible, I would be guided to find a solution that is satisfactory.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-14 4:17 AM
Dear @Cnnon.1 (Community Member)
Could you give more details to the STM32 Community about the material you use (HW and SW, tools and versions, board(s), motor(s) and so on)?
Best regards
Laurent Ca...