cancel
Showing results for 
Search instead for 
Did you mean: 

MCSDK– How to analyse SW & HW

JayarajAnbalagan
Associate II

Hai All,

  New to MCSDK Tool – 446 + IHM08M1 Interface.

Generated the code using MCSDK 6.4.1 and analysing it.

Attached is the video of my motor control configuration – Basic Hall Effect Sensor based 6 step commutation using Switch and ADC Speed Control.

Unable to see any control routine in my main closed loop – where the switch press and the speed control ADC is called.

Kindly help me out, how to proceed.

1 ACCEPTED SOLUTION

Accepted Solutions
STuser2
Senior III

I think it will not be part of the main while loop, it will be part of other user related application files.

View solution in original post

3 REPLIES 3
STuser2
Senior III

I think it will not be part of the main while loop, it will be part of other user related application files.

Sir,

  That is correct. Connected the Motor with the generated code, it spins.

How to make use of the ST Motor Pilot?

Does it Auto detect the Hardware or we have to manually feed?

Configured a serial port in my generated code with 19200 Baud Rate.

You have to open the motor pilot and then click on Discover Board then it will auto detect i think.