cancel
Showing results for 
Search instead for 
Did you mean: 

MC_SetCurrentReferenceMotor1( qd_t Iqdref )

PGinhson
Associate III

I need help with the code generated by the workbench.
I am using the STEVAL-CTM01xV1 shunt code with the STEVAL-CTMo11V1A development board and the STLINK/V3 with the isolator adapter.
Following the instructions that appear in the comments of mc_api.c, I added the three routines before the main while:
MC_ProgramSpeedRampMotor1(1000,250);
MC_ProgramTorqueRampMotor1(935,200);
MC_SetCurrentReferenceMotor1();
In the last routine, it is not clear what the parameters, units, etc. are like.
Documentation is missing or at least I can't find it, I need more information to be able to continue with the development.

Blessings on your courage, that's the way to the stars
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
GMA
ST Employee

Hello,

You can find implementation details on mc_api.c MC_ProgramTorqueRampMotor1 function header that mention that this function sets Iq current value.
Using MC_SetCurrentReferenceMotor1 function, you have to set a "qd_t Iqdref" parameter that represents Iq and Id. 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA