2020-03-26 08:10 AM
The Workbench can only generate code for sensorless or quadrature/hall sensors. Can the controller be fed with position values (received via SPI for example) or is this not intended?
My particular usecase is: The motor to be used has a BISS encoder and is intended to be driven slowly, but precisely. hence it would make sense to use the BISS encoder.
2020-04-03 05:29 AM
Hello Leonlf,
Yes adding resolvers is part of our roadmap.
Thanks and best regards,
Claire
2020-04-03 09:08 AM
The sdk datasheet implies user-made encoder code. As the quadrature encoder code is _weak attributed, can I just override the getPosition methods?
Would the delay disturb the controller?
2020-10-15 06:24 AM
Dear @Leonelf
Do you have still this problem to solve?
And just in case, if not, do not hesitate to share the final solution you found.
Best regards
Laurent Ca...
2020-10-22 05:51 AM
has there been an update as to when it will be implemented?
2020-10-22 06:06 AM
Dear @Leonelf
Could you give more details to the STM32 Community about your setup -the material you use- (HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)?
And more especially did you use MC tools (such as MC_suite, MC-Motor Profile, MC-SDK, MC-workbench, and so on)?
Best regards
Laurent Ca...
2020-10-26 01:56 AM
Dear @Leonelf
Any news?
Best regards
Laurent Ca...
2020-11-02 12:09 AM
Dear @Leonelf
As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...
2020-12-14 04:59 AM
@Laurent Ca...
I'm looking into the same use case for an absolutt biss encoder as @Leonelf . Do you have any updates regarding an "absolutt encoder implementation" in the STM firmware?
thanks
mr. andy
2021-03-10 09:50 PM
Dear @mrandr
It is a rather old question.
Please open a new one in adding reference to this one.
Best regards
Laurent Ca...