cancel
Showing results for 
Search instead for 
Did you mean: 

IHM14A1

Jerome_DataP
Associate

Hello,

I would try to use  the IHM14A1 shield  and  for now i only have a nucleo F2 series . it seemed in the document that this nucleo is not supported , can somebody tell me if it can't works  or maybe with some modifications on the example code.

 

thanks 

jerome

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hello @Jerome_DataP and welcome to the ST Community.

From the hardware point of view you can use a Nucleo F2 series board to drive the X-NUCLEO-IHM14A1 shield.
You can use generic GPIO to drive the motor driver expansion board.

There are no libraries ready for this pair of boards, in fact the X-CUBE-SPN14 software is compatible with a selection of Nucleo board.

 

If you feel a post has answered your question, please click "Accept as Solution"