2018-02-27 1:19 AM
In UM1052 it says that ICS current sensing is only available for F103 HD, F2xx, F4xx. However the class ICS_F30X_PWMnCurrFdbk is part of the MC Library.
Is this class with it's functionality a work in progress? It does not compile as reported here:
It seems that development of this class is started but not finished. But why include unfinished non-working SW in the lib? What is going on here?
I wish to run F303 single motor control with a 2-shunt inline current sense topology.
#sw #ics #f303re2021-06-28 2:41 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.