2020-03-25 7:45 PM
I have set the jumper pins with respect to the user manual.
The motor only runs after I profile it at the motor profiler, when I run the program into the board using the STM32CubeIDE, the motor stops running again. And when i want to profile it again it says that a firmware upgrade is needed for the board to connect to the profiler.
2021-06-27 9:38 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards