Associate III
September 9, 2024
Question
HSO Evaluation Problems
- September 9, 2024
- 1 reply
- 1232 views
Dear All,
My platform as list:
Control Board: B-G473E-ZEST1S
Power Board: STEVAL-LVLP01
Motor: B-MOTOR-PMSMA1
Platform: MCSDC 6.3.0, (I attached my Workbench configuration file as follow)
CubeIDE: 1.15.1
When I try to evaluate the HSO, the Motor pilot appear in weird value.
The speed reference and mechanical speed is wrong.
Also, there are a orange waring, "Access Register of Bus Voltage resulted in error" on the buttom.

Once I start the contol, it will occurs "Over Current Fault"

Has anyone encountered a similar issue? How can it be resolved?
Best Regards,