cancel
Showing results for 
Search instead for 
Did you mean: 

How to use MC Workbench with STM32F303 & LQFP48 package

peterpeter9162
Associate II
Posted on September 08, 2016 at 23:19

Hi,

I've been working with MC workbench and want to use a smaller package STM32F303.  However, the project configuration for analog inputs only offers pins that are not available on the LQFP48 ''C'' package.  I have no wish to use the 64 or 100 pin package for a small simple application.

Can I use the STM32F303CB part? 

Thanks in advance.

#stm32f303-mc-workbench
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards