2022-02-25 2:09 PM
I use STM32CubeIDE (1.5.0) as a toolchain without a current CubeMx file. What is the means of upgrading motor drivers from 5.4.4 to 5.Y.4?
I have done the basic install of 5.Y.4 under folder C:\Program Files (x86)\STMicroelectronics but in my CubeIDE project the drivers are duplicated under folder:
C:\Users\Brian\ST_workspaces\Bitbucket - repo -v03.10.02 - New_Filter\cascade_pfd\Prysm_Test_Board_LL
I tried replacing the 5.4.4 folder in my project with the 5.Y.4 folder but get a build error.
I then edited the path in Project//Properties/Paths to the new folder location of 5,Y.4..
Are there any notes somewhere to go through the steps of upgrading the motor drivers?
Thanks,
Brian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.