cancel
Showing results for 
Search instead for 
Did you mean: 

Can STEVAL-SPIN3201 be programmed for sensorless 6step? I try to use X-CUBE-MCSDK-Y (6S_STEVAL3201_SL_VM) but when i use the Keil and download it to the board, the motor don't work and i can't connect to the motor pilot 5.Y.1

LTren.1
Associate

Hi ST Community,

I'm seeking to start a motor with FOC and six-steps to analyze the difference. When i used the FOC example it works fine, but when i change something and download it to the board with Keil the motor control workbench don't connect: Connection failed! No response, check the communication cable...

At least the example BullRunning works, but the 6steps (6S_STEVAL3201_SL_VM) do nothing

What I'm doing wrong?

what i can do to change configurations on the BullRunning and still connect the board to the motor control workbench?

To use 6steps, i need to change something on the board?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK). 

Best regards