How to choose the Timer Input Capture Filter value
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-01 8:55 AM
I'm using an STM32 to control a DC motor with a dual hall encoder feedback.
To monitor motor position I want to use a General Purpose Timer (16bits) in Encoder Mode.
As my input is noisy, I want to filter the signal using the Input Capture filter.
My problem: I don't find any information about the ICTimer.
Here's what I found in the AN4013 - STM32 cross-series timer overview Application note
> "Program the filter by writing the IC1F[3:0] bits in the CCMRx register, and the prescaler by writing the IC1PSC[1:0] if needed"
What kind of filter is this?
How do I choose the value for IC1F?
What is the cutoff frequency?
Your help is appreciated.
Solved! Go to Solution.
- Labels:
-
STM32 Motor Control
-
TIM
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-01 3:39 PM
I fail to see how this works as a filter.
The following figure from AN4776 illustrates how the input capture filter rejects short pulses (i.e. noise):
It's not a perfect solution, of course. It introduces delay, and it's aimed at removing random switching noise not periodic interference (in which case it may produce confusing results).
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-01 9:54 AM
You are not specifying the chip, so I took G4 series as an example. Ref. manual RM0440 Rev 6 says in 28.3.9 Input capture mode "Let’s imagine that, when toggling, the input signal is not stable during at must 5 internal clock cycles. We must program a filter duration longer than these 5 clock cycles.". So the filter is just debouncing transient transitions. It is named "Filter downcounter" in the figures.
ICPS is a prescaler. No idea what it is used for except for extending the counter range.
hth
KnarfB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-01 10:33 AM
Which STM32?
> As my input is noisy
Specify.
> What kind of filter is this?
It's very simple: if input level changes, output changes only after filter samples the same level for the prescribed number (N) of samples. You can select several levels of N and several prescalers for the sampling frequency.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-01 10:43 AM
Wouldn't the prescalers divide the input pulses, so you'd need 4 or 8, or whatever, to get a single count?
The clock divider of the filter drops the sampling frequency, ie clocking of the synchronizer circuit
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
‎2022-03-01 12:46 PM
Sorry for the confusion with the many prescalers:
- there is a common prescaler for filters in all 4 channels (and for dead-time detection where applicable), set in TIMx_CR1.CKD (resulting in fDTS)
- individual settings of TIMx_CCMRx.ICxF use a further subdivision of either directly the timer's internal clock (***_INT) or its prescaled version (fDTS)
- as Clive said above, IC1PSC determines, after how many filtered edges will an actual capture occur.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-01 1:37 PM
Hi @Community member​ ,
Thanks for you answer.
> It's very simple: if input level changes, output changes only after filter samples the same level for the prescribed number (N) of samples. You can select several levels of N and several prescalers for the sampling frequency.
What you're describing seems like a counter.
If it's the case, how is the hysteresis working?
> as Clive said above, IC1PSC determines, after how many filtered edges will an actual capture occur.
From my observation, I don't think it's the case.
The filter seems to behave like a low pass filter: filtering out rapid variations, regardless of the number of edges.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-01 1:47 PM
> What you're describing seems like a counter.
You can look at it as a counter. This is exactly how debouncing algorithms work in software, too.
> If it's the case, how is the hysteresis working?
What hysteresis are you referring to?
>> as Clive said above, IC1PSC determines, after how many filtered edges will an actual capture occur.
> From my observation, I don't think it's the case.
> The filter seems to behave like a low pass filter: filtering out rapid variations, regardless of the number of edges.
ICxPSC does not control the filter itself.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-01 2:33 PM
Hi everybody,
I think I don't understand what you're saying.
When I implement a low pass filter with a counter, I put two hysteresis thresholds.
Here's a rapid drawing about the relationship between the input, the counter and the output.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-03-01 3:39 PM
I fail to see how this works as a filter.
The following figure from AN4776 illustrates how the input capture filter rejects short pulses (i.e. noise):
It's not a perfect solution, of course. It introduces delay, and it's aimed at removing random switching noise not periodic interference (in which case it may produce confusing results).
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-26 11:32 AM
The AN4776 had the details needed.