How to change the MCSDK5.4.0 default speed step (6) to one(1) ?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-11 11:49 PM
In the MCSDK5.4.0, I want to improve the speed resolution ratio,the default is six;
I change the file of mc_stm_types.h, change the default SPEED_UNIT from _01HZ to _001HZ ;and the _RPM from 60 to 100. When I call the api MC_ProgramSpeedRampMotor1(600,4000),the motor can not work,but the pMCI[0]->hFinalSpeed is correct。When I use the _RPM default 60, the motor can work ,but the speed is wrong
Labels:
- Labels:
-
STM32 Motor Control
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-06-27 10:16 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards