2019-11-21 12:12 AM
The Motor runs correctly when i am driving it from serial through MC WB. but i want to drive the motor from PWM.
Any Help Plz...
2020-05-22 10:48 PM
Hi Nain,
did you manage to resolve this issue please?
I have a similar toolchain setup (albeit a couple of slightly updated versions) and get the same response.
Motor runs perfectly under ST Motor Profiler and ST MC Workbench, but when code is generated for EWARM 8, compiled and pushed out onto the chip there is no response to 490Hz PWM input with 1240us duty.
Any indication of how you corrected the setup/ configuration/process would be greatly appreciated.
Regards
Tim
2021-06-27 10:18 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards