cancel
Showing results for 
Search instead for 
Did you mean: 

Getting source files for PWM interface

jorge2
Associate II
Posted on April 20, 2016 at 21:40

Hi,

I am building my own motor control libraries, and I need an example of the PWM interface. Looking at the FOC SDK, this function, and others like this one, is of interest to me:

uint16_t PWMC_SetPhaseVoltage(CPWMC this, Volt_Components Valfa_beta);

How can I get the source files for this function? It seems to be embedded in a library, but this shouldn't have any IP, since it is just a peripheral interface. Thanks for the help!
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Gigi
ST Employee
Posted on April 21, 2016 at 08:32

Ciao

You have to ask the source code to your nearest ST distributor.

Ciao

Gigi

jorge2
Associate II
Posted on April 21, 2016 at 16:50

Thanks, how can I find my nearest distributor? Do you have an email or phone number?

jorge2
Associate II
Posted on April 21, 2016 at 17:37

Never mind, I see the map on st.com, so I will give them a call.

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards