2016-04-20 12:40 PM
Hi,
I am building my own motor control libraries, and I need an example of the PWM interface. Looking at the FOC SDK, this function, and others like this one, is of interest to me:uint16_t PWMC_SetPhaseVoltage(CPWMC this, Volt_Components Valfa_beta);How can I get the source files for this function? It seems to be embedded in a library, but this shouldn't have any IP, since it is just a peripheral interface. Thanks for the help!2016-04-20 11:32 PM
Ciao
You have to ask the source code to your nearest ST distributor. Ciao Gigi2016-04-21 07:50 AM
Thanks, how can I find my nearest distributor? Do you have an email or phone number?
2016-04-21 08:37 AM
Never mind, I see the map on st.com, so I will give them a call.
2021-06-15 07:16 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards