2020-01-16 5:49 PM
After Workbench and Keil firmware was doenloaded to STM32F103RC. But it showed Unkown error when I tried to run the motor via Worknench. When stop run button was clicked it show "any stop". Anyone can tell me what happened and what should I do? Thank You
2021-06-14 11:37 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards