cancel
Showing results for 
Search instead for 
Did you mean: 

do I really need CubeMX?

dsamm
Associate III

I've recently done a clean install of STM32CubeIDE, and after went for the x-cube-mcsdk setup.

The motor WBench cant generate the code because CubeMX is not installed...

But in fact CubeMX is now embedded in STM32CubeIDE.

How can this issue be solved? (see screenshot )

-d

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The integrated CubeMX is not accessible from the outside. But you can easily install the stand-alone version of CubeMX in parallel with CubeIDE. They even share the same repository if you set the path to the repository the same for both.

When your question is answered, please close this topic by choosing Select as Best.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

The integrated CubeMX is not accessible from the outside. But you can easily install the stand-alone version of CubeMX in parallel with CubeIDE. They even share the same repository if you set the path to the repository the same for both.

When your question is answered, please close this topic by choosing Select as Best.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.