cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot enter HRTIM1_Master_IRQHandler

AZaya.1
Associate

Hello, I'm using STM32F334C8T6 and trying to measure the duration of my calculation section

from MCMP1R (JEXT9) which triggers ADC1 till all TIMER's D CMP registers change.

1) I enabled Global Master Timer Interrupt and MCMP1 interrupt

NVIC_EnableIRQ(HRTIM1_Master_IRQn);

 NVIC_SetPriority(HRTIM1_Master_IRQn,1);

 HRTIM1->sMasterRegs.MDIER |= HRTIM_MDIER_MCMP1IE;

2) I made the Master Timer Settings in such way:

HRTIM1->sMasterRegs.MCR |= HRTIM_MCR_CK_PSC_0; // 128 MHz * 16

HRTIM1->sMasterRegs.MCR |= HRTIM_MCR_CONT;

HRTIM1->sMasterRegs.MPER = PERIOD; // 40 KHz PWM

HRTIM1->sMasterRegs.MCMP1R = 1024; // 0.5 microseconds

HRTIM1->sCommonRegs.ADC2R |= HRTIM_ADC2R_AD2MC1;

3) And finally the IRQ handler, which doesn't work

void HRTIM1_Master_IRQHandler(void)

{

if(HRTIM1->sMasterRegs.MISR & HRTIM_MISR_MCMP1)

{

HRTIM1->sMasterRegs.MICR |= HRTIM_MICR_MCMP1;

DWT->CYCCNT = 0; //Start of measuring

 }

}

Please help, where the proglem is

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

Dear @AZaya.1​ 

Welcome to the STM32 Community

Could you give more details to the STM32 Community about your setup -the material you use- ?

(HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)

And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, and so on)?

Best regards

Laurent Ca...