cancel
Showing results for 
Search instead for 
Did you mean: 

How can I reduce the RAM consumption of AER applications?

Fyouj.1
Associate II

Dear ST Engineer,

I use CubeMX. AI debugging the AER applications downloaded from https://github.com/Shahnawax/AER-CNN-KERAS, need RAM 9.31 MiB, no matter use what kind of compression is so big, that is to say there is no that kind of MCU can adapt to this kind of use,What can be done to reduce RAM consumption?Or is there any MCU that has that much RAM?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

Is this even designed for an MCU target, or an embedded linux platform?

You might need code the algorithm yourself in more efficient manner, in native code.

For high RAM requirements, perhaps look at the STM32 DISCO boards with SDRAM

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Guru

No STM32 MCUs have 9MB of built-in RAM. You could add an external chip such as SDRAM to accommodate this. However, it seems like the application you are running is not intended for an embedded platform.

If you feel a post has answered your question, please click "Accept as Solution".